-
Chain Wear Gauges are high-quality, robust, and durable. The Chain Wear Gauges enable precise measurements where traditional calipers cannot be used. They are suitable to measure BS and ANSI standard roller chains.
-
The Tube and Pin Oven Repair Tool can act as a replacement of conveyer pins.
-
This chain breaker can be clamped in a vice or screwed onto a workbench. To use, position it at the front edge of the bench to provide enough space for the lever to swing down fully. If set correctly, both chains with shouldered and chains with straight pins can be broken. The rotating head holds five sets of ejector tools which is marked with the respective size of the chain.