This chain breaker can be clamped in a vice or screwed onto a workbench. To use, position it at the front edge of the bench to provide enough space for the lever to swing down fully. If set correctly, both chains with shouldered and chains with straight pins can be broken. The rotating head holds five sets of ejector tools which is marked with the respective size of the chain.