-
The ELITE Leaf Chains are used wherever loads must be lifted, hoisted or pulled with high fatigue strength. The most common use of ELITE Leaf Chains are in forklift truck masts, but they are also used as a counterbalance chain in machine tools. The chain plates are tapered and shot-blasted which allows them to have high contact ratios.
-
The ELITE Accumulation Roller Chains are used for conveying goods on lines that stop and start intermittently while the chain continues to run. As the external rollers on one side of the chain mesh with the sprocket teeth to transmit drive power, the other side supports the chain in the guide profile.
-
The ELITE Rubber Top Roller chain are ideal for applications where fragile goods require gentle conveyer handling. This chain can be used for transporting goods that should not be scratched. This ELITE chain is made with nitrile butadiene rubber with a hardness of 80 shore.