-
The ELITE Accumulation chains are used for conveying goods on lines that stop and start intermittently while the chain continues to run. The external rollers on one side of the chain mesh with the sprocket teeth to transmit drive power while on the other side, they support the chain in the guide profile.
-
The ELITE Accumulation Chains with Finger and Parts Protection are fitted with 100% protective tab between the accumulation rollers, which covers the gap in the inner link area. This feature offers protection against particles falling through the gap, which could lead to the jamming of accumulation rollers.